12/9/2024 11:03 AM | |
Joined: 12/12/2023 Last visit: 12/23/2024 Posts: 4 Rating:
|
Here is the promised picture with the settings |
12/11/2024 10:25 AM | |
Joined: 10/11/2006 Last visit: 4/17/2025 Posts: 6008 Rating:
|
Hello, The Web server is addressed via HTTP/S. FTP and Telnet are only connected to the user administration. Security concept of HTTP/S, FTP, and Telnet access on the Web server As of version V4.4, access to the SIMOTION IT Web server is protected by a multi-level security concept. The security state of the Web server is indicated by the security level on the Website. There are three possible security levels: Low, normal, high. You will find detailed information on the security concept of the connection via FTP/Telnet in the SIMOTION IT Diagnostics and Configuration Diagnostics Manual, section "Security concept" 3.3 Activating communications services in SCOUT TIA https://support.industry.siemens.com/cs/ww/en/view/109963298 |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on