7/19/2017 2:05 PM | |
Joined: 9/27/2006 Last visit: 3/26/2025 Posts: 12344 Rating:
|
Hello Jacplacu; Do you have screenshots of the network view or a copy of the diagnostic buffer we could examine, to help sort out the problems you seem to have? The connection of a standard Profibus cable to a standard Profibus connector is very simple and described in many locations in Siemens documentation. For example, look at section 4,2,2 in this manual: PROFIBUS Networks - Siemens Support Many things can happen to cables in a plant, from lightning strikes to the famous forklift accident... Those are generally easy to catch. What can happen with Profibus cables and connectors on installation or after operating a while? - wires A (Green) and B (red) on the Profibus cable could be crossed (reversed)from one connector to another. - the shield connection (on the Profibus cable) could be loose in the Profibus connector (it must be pressured by the connector body when you screw the connector shut); if the ground connection is not maintained over the length of the network cable tranmssion will be impeded. Sometimes vibrations will cause the shield to become loose in the connectors; continuity tests will reveal that. - the terminating resistance must be ON (and powered) for the 2 end stations of the bus: the first and the last node (physically) must be be powered and the terminator at ON. Loss of the termination will cause the whole network to crash, because the terminators eliminate reflexions on the bus; reflexions will disrupt transmissions. Always check that the end nodes are powered; if you need to take one down for maintenance, place the terminator on the closest station to ON (or use an externally-powered termination module. For more information. these documents could be of interest to you; they are produced by Profibus.com (Profibus International -PI), the governing body of all thisng Profibus and Profinet: Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/19/2017 2:07:19 PM |
|
Follow us on