9/12/2018 9:22 AM | |
Joined: 11/1/2016 Last visit: 6/9/2022 Posts: 10 Rating:
|
Hi friends,in our plant ,i have two machines similar . The HMI of theese two machine are SIMATIC PANEL PC 677B . One of theese hmi has damaged . the disk Inside the PC is damaged so i changed by another one and i think if i make a copy of the .FWX file in the new hard disk and with the same software wincc runtime 2007 .it will be a good solution ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/12/2018 12:46:57 PMNew subject after splitting |
|
Follow us on