6/29/2017 9:53 PM | |
Posts: 352 Rating:
|
Hello, Sounds like your Profinet name might be wrong.. Kind regards Ola |
6/29/2017 11:04 PM | |
Joined: 8/5/2015 Last visit: 2/11/2022 Posts: 5 Rating:
|
Hello and thanks for the answer What do you mean? Repeated? Used? |
6/30/2017 1:50 PM | |
Joined: 8/5/2015 Last visit: 2/11/2022 Posts: 5 Rating:
|
Hello. I'm 100% sure names are differents and IP address is well assigned and to only one device |
7/1/2017 8:30 AM | |
Joined: 8/31/2013 Last visit: 3/8/2025 Posts: 607 Rating:
|
Hi I have GSDML file for Danfoss Profinet this file working without any problems with S7-1200 AttachmentDanfoss.zip (633 Downloads) |
Last edited by: MAZENJER at: 7/1/2017 8:30:46 AMWarm Regards |
|
This contribution was helpful to
1 thankful Users |
7/3/2017 2:04 PM | |
Joined: 8/5/2015 Last visit: 2/11/2022 Posts: 5 Rating:
|
Thanks, let me try |
11/24/2017 3:33 PM | |
Joined: 9/27/2006 Last visit: 3/18/2025 Posts: 12344 Rating:
|
Hello phuongdt; This thread discusses Danfoss drives (FC 102) over Profinet. So here ia a Danfoss manual showing how to use Profinet with this drive, how to parametrize it, how to configure the network and how to exchange data and commands between the PLC and the drive. Section 7.4 shows a small example of one Hardware configuration for this drive in the PLC (over Profinet) and the read and write instructions between the PLC program and the drive. http://www.algoritm-tula.ru/catalog/danfoss/doc/fc103/profinet-rt-mca-120-programming-guide.pdf |
Follow us on