7/12/2006 1:02 PM | |
Posts: 43 Rating: (0) |
it is strange i can see alarms, but when i came to tags i get that error. I did put all security settings on enable, but this did not solve my problem. |
7/12/2006 1:12 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
That is odd. Usually both work or none work ! What versions are you running (Windows, IE, WinCC, DataMonitor) ? |
7/12/2006 1:21 PM | |
Posts: 43 Rating: (0) |
i am using following software: -Win2000 Server SP4 (build 2195, sp4) -Wincc V6.0 SP4 -WebNavigator Server /Client V6.1 SP1 -Dat@Monitor Server/Client V6.1 SP1 |
7/12/2006 1:23 PM | |
Posts: 43 Rating: (0) |
sorry, and IE 6.0 SP1 |
7/13/2006 9:50 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
A few more questions, if you will ... |
7/13/2006 10:12 AM | |
Posts: 43 Rating: (0) |
1)Add http://localhost as a trusted site and then try connecting to URLhttp://localhostinstead of ip address or computername. Does this make any difference? I done this but same happens 2) Have you tried connecting from another computer ? I think the problem is either with the IIS settings or IE settings. Another computer (preferably running another operating system) would help rule out IE settings. when i try to connect from other computer, browser stucks on that computer, but i think thats problem with webclient 3) What happens if you use the"Tag data on a trend"link(instead of "on a table") ? Same thing happens like with "Tag data on a table". |
7/13/2006 10:49 AM | |
Posts: 43 Rating: (0) |
This did not solve problem, i still see in corner error"done but with errors on page", when i see details error is same Thanks, Sukrija |
7/13/2006 11:14 AM | |
Posts: 43 Rating: (0) |
Yes i get data which i configured to view. So DatWorkbook works |
7/13/2006 12:01 PM | |
Posts: 43 Rating: (0) |
DatWorkbook is working from webnavigator too. i will try install on another machine. |
Follow us on