2/23/2013 5:30 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
How do you program the TSEND_C and TRCV_C instructions for open user communication over the integrated PROFINET interface of the S7-1200 CPU? |
2/24/2013 1:42 PM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello SegersM, You cannot do it as easy as PROFINET works, as all 4 are PROFINET IO Controllers (all the 4 CPUs) in your case. You can still exchange data between CPUs using T Communication (TCP/IP) Have a look at this application example which deals about the similar situation. - Ethernet Communication: Data Exchange S7-1200 <-> S7-1200 (CE-X17) |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on