2/15/2021 7:54 PM | |
Joined: 7/2/2015 Last visit: 4/24/2025 Posts: 96 Rating:
|
Dear Dongerpure, The script that you means works on a PC because a PC has Windows standard and a panel has a Windows CE. So you need to use CreateObject("FileCtl.File") as it said at point 4 <line 35> of the FAQ "With SIMATIC WinCC (TIA Portal) on a panel, how do you access process data in a file via a script?"
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
2/16/2021 7:50 AM | |
Joined: 3/8/2011 Last visit: 5/17/2023 Posts: 262 Rating:
|
Thank you its working if we want every parameter in different column then??
|
If this post helped you, you may use the Rate-button |
|
Follow us on