9/6/2017 8:23 AM | |
Posts: 2 Rating:
|
Hello everyone, I am having some issue to process data from a Bizerba iS30 through Profinet, as shown on the pictures attached. Indeed, the data are successfully read and are copy to a DB using DPRD_DAT (REAL, BYTE, etc.). However, this doesn't work for the Struct type of my DB. I imagine it has to be copied to a word using DPRD_DAT and then transfered bit by bit. My issue is there : how can I copy the data of a word into a struct of 16bits? I already tried to use a MOVE or MOVE_BLK without success and I only have FieldRead or Fieldwrite available under "Legacy", which is likely due to the basic function of our S7-1200. Thank you in advance for your help! AttachmentPictures_issue_Data processing_Word_to_Struct_16bits.pdf (78 Downloads) |
Follow us on