1/4/2011 11:00 AM | |
Posts: 8 Rating: (0) |
I have had a similar problem with warning 300:9. Solve in your manner. Thank you |
1/9/2017 1:05 PM | |
Joined: 12/18/2006 Last visit: 8/31/2023 Posts: 89 Rating: (6) |
I have also have issues displaying project hierarchy and I have broken the multiproject a couple of times when I have accessed it from a ES over the ethernet. The "master" project is situated on a IPC with 64bit Win2008R2. The "remote" ES is a Field PG M4 64bit Win7Ult. (Do not know if the OS-difference causes the issues, because we have not had any problems with Win2008R2 "remote" ES's). However, when the hierarchy was not shown, I saw that the Simatic workplace server (hammer icon) was not running on the remote ES and it was not possible to start the server. When I set it to Single terminal system, it did start and the hierarchy worked. I'm not sure on what effect this has to the project so I set it back to Multi-user. PCS 7 PCS 7 - PC Configuration (V8.1 SP1) chapter 5.4.4 How to prepare the engineering station for multi-user operation contained information on Setting up the Sybase server as a service. The manual does not say clearly why you would have to set this up. Setting it as a service on the remote ES made the hammer-icon disappear but the hierarchy of the project works so this might be a solution if you have this issue. |