10/1/2016 11:36 AM | |
Joined: 12/7/2009 Last visit: 4/23/2025 Posts: 33 Rating:
|
Hi Milosh, --> What do you mean by share everything under private and public? Assuming you have Win 7 installed on both Server & client side, just have a look at "Sharing options.jpg" to get exact Idea on where you can set the sharing options. --> Sorry, what is Simatic shell I never use it. Where to find? Again assuming you have Win 7 in server, simplest way is to just open "My Computer" or "Computer" from stat menu or Windows Explorer (Press Windows Key + E) & the last Icon in that you find in that window is "Simatic Shell". Relevant screenshots are "Simatic Shell.jpg" & "Simatic Shell Folder.jpg" --> Create password and user for client pc, you mean, on server defined user DM_Demo in computer management, and also make same user on client pc, with same password and same groups? Basically you need to have access to server from client. In such case I prefer to create user only in Server windows, give the user specific rights & add the user in relevant groups, create same groups in client windows also & connect the client to the domain & login with the User name password created in server. Later you can use the DM_Demo credentials for web access. Could you give more details on the OS on both the computers & Antivirus installed? AttachmentScreenShots.zip (227 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on