4/13/2018 9:36 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello First of all The comfort Panels are not able to perform an automatically switching of the Daylight saving time by itselfs. You only can activate or deactivate the DST (daylight Saving Time). Also the Checkbox in the Settings only activates it but ther is no automatically switch. The S71500 for example is able to do this. So you have to use a little workaround to trigger this on the Panel by Systemfunction: https://support.industry.siemens.com/cs/de/en/view/109482675 And here is the Basic FAQ for all remaining questions: https://support.industry.siemens.com/cs/ww/en/view/69864408 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
3 thankful Users |
Follow us on