3/1/2014 11:20 PM | |
Joined: 4/11/2011 Last visit: 4/11/2023 Posts: 132 Rating:
|
First: Procedure To set the block access, proceed as follows:
Then do compile. Now you have DB with offsets. In "Program blocks" copy your DB and paste. Now you have two DB-s with different names but same DB nr. e.g. "Data_block_1"[DB1] and "Data_block_2"[DB1] Open second DB ("Data_block_2"[DB1]) and rename "alarm1" to "alarm3" etc. Delete first DB ("Data_block_1"[DB1]). Rename second DB as first -"Data_block_1". Symbolic addressing remains the same but absolute is changed. Some pictures AttachmentDB.pdf (201 Downloads) |
I'm just a human. Mistakes are allowed. |
|
This contribution was helpful to
1 thankful Users |
3/2/2014 2:35 AM | |
Posts: 43 Rating:
|
Interesting idea. I am going to give it a shot and report back. Thanks for the idea. Never thought of that one. |
Follow us on