4/12/2017 9:16 AM | |
Joined: 5/15/2010 Last visit: 2/8/2024 Posts: 172 Rating: (3) |
Hi Experts, We are commissioning Sinamics S120 system where we are using 4.8V CF card (with and without performance). We are using unsigned double integer to real block. After publishing all connections and compiling we are able to see the double integer input to the block (online), the processed output of the block is always zero. We have tried with V4.60.6.0/V4.70.7.0/V4.80.11.0 libraries. We have used V4.6 CF card and the block is processing. I have also attached software. AttachmentTestLogic.zip (29 Downloads) |
4/12/2017 9:34 AM | |
Joined: 5/15/2010 Last visit: 2/8/2024 Posts: 172 Rating: (3) |
Hi, I cannot find the context menu in DCC. Please suggest the path. |
4/12/2017 9:52 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980)
|
RTFM! right click on the DCC Chart in starter! |
4/12/2017 11:39 AM | |
Joined: 5/15/2010 Last visit: 2/8/2024 Posts: 172 Rating: (3) |
Done and now its working. Thanks.. |
Follow us on