7/2/2014 8:15 AM | |
Joined: 12/29/2012 Last visit: 2/6/2024 Posts: 120 Rating: (15) |
Dear Techteam, Thanks for immediate response ,now i create one DCC chart for Simple Function , I use one AND Gate function, Input For AND is coming from Control unit and Output is connected to the DO8. When i compile the logic i found an error, input and output must be published, Here with i attched the Error image,Please Help me To Solve this Issue Thanks in advance. AttachmentPROBLEM.zip (137 Downloads) |
Last edited by: Narrator1 at: 7/3/2014 5:45 PMTopic split from /tf/WW/en/Posts/110859#top Best regards |
|
3/18/2015 5:48 PM | |
Joined: 3/14/2013 Last visit: 12/15/2021 Posts: 5 Rating: (4) |
Dear all. Some times, it´s hard to get a compreensive help. I study a lot, and always as possible, I try to help my colegues (as I would like to receive help too). Siemens, is simple, but you need to study. Regarding the question of colegue, I am sending a SIMPLE DCC EXAMPLE. I hope that it help you. Regards, Anderson.
AttachmentDCC_SIMPLE___.pdf (431 Downloads) |
This contribution was helpful to7 thankful Users |
Follow us on