1/23/2018 7:38 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello evertonjc, Please provide detail information. Have you purchased standard DCM & tried to commissioned? Are you facing problem of F60069? Please check the fault value in r0949 & inform here. Do you have any specific Di/DO or AI/AO requirement other than the standard? Siemens must have explained you the reason to go for advance control unit. Is your motor is with PM field? or your motor field current is much high than the present DCM field current rating? In above case, please provide complete drive MLFB & motor name plate details (preferably name plate snap) along with motor application details, so as to help you. HTH |
1/26/2018 10:11 AM | |
Joined: 9/16/2013 Last visit: 5/28/2024 Posts: 199 Rating:
|
if you want to use a sinamics DCM with profinet you must use a Advanced CU + CBE20 |
Follow us on