5/12/2021 1:38 PM | |
Joined: 4/10/2006 Last visit: 4/14/2025 Posts: 959 Rating:
|
Hi, when I type a value in a numeric field on the operator panel I then press ENTER to confirm it ... I have the problem that the field is always active and the blue field does not disappear. what can i do to deactivate this field after typing the value and pressing enter? I attach pdf with some images: you can see the field still active after typing the number and pressing enter. you can see the inactive field because I moved elsewhere. I need to deactivate this enabling because in this way I can use the "activate" and "deactivate" functions in the input field, under "properties" ----> "events" Is it possible to move the focus somewhere else after entering the data???? Thank you Roby Attachmentalways aktive field_small.pdf (85 Downloads) |
Last edited by: Roby at: 05/12/2021 18:04:14Setting of my PG M6 Siemens |
|
5/13/2021 9:35 AM | |
Joined: 6/19/2019 Last visit: 4/18/2025 Posts: 721 Rating:
|
Can you share your experence and tell us how you do that? |
This contribution was helpful to
1 thankful Users |
Follow us on