2/11/2020 9:45 AM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating: (1359)
|
|
This contribution was helpful to1 thankful Users |
2/11/2020 5:55 PM | |
Joined: 3/5/2013 Last visit: 11/2/2022 Posts: 7 Rating: (1) |
@hdhosseini Apologies I didn't realize DEAD_TIME was a standard block. The library path in original screenshot was not one I recognized. I misunderstood, thought this was something you had implemented in SCL. Now I understand it is standard block in PCS7 library. I assume you get this library with an installation of PCS7, do you know if you can download this library for free from Siemens website? Also, I post here my solution, see FIFO.zip FC314 (STL implementation) is FIFO function, max buffer 100 Reals. You pass DB number, assumption is start address is 0. it calls FC214, function from our code base - limit check. FC214 is included in library. Also calls Simatic SFC24 to check DB validity and length. Michael PS Your video channel looks very interesting. I will have a look. AttachmentFifo.zip (84 Downloads) |
Last edited by: m_c at: 02/11/2020 17:56:16 |
|
This contribution was helpful to1 thankful Users |
2/11/2020 10:57 PM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (106) |
Hello m_c, Maybe this post can help as well, in combination with
FIFO [store Data DB into Buffer DB] Best Regards Soble |
Last edited by: SOble at: 02/11/2020 23:00:18Last edited by: SOble at: 02/11/2020 23:01:31Website: |
|
This contribution was helpful to1 thankful Users |