11/6/2008 1:38 PM | |
Posts: 5822 Rating: (412)
|
Dear Phi, well, the use of handshakes for your communication is really important, because only that way you may warranty a tough performance on the bus. If I just think about FETCH / WRITE you may receive the requested data within less than 100 ms. Have you seen the sample about the FETCH / WRITE for the PN CPU yet? Implementation of the FETCH/WRITE service in an S7 CPU with PROFINET Interface Maybe it can give you some idea. Best regards J_Bell |
11/6/2008 4:26 PM | |
Posts: 5822 Rating: (412)
|
Dear Phi, this sounds great, I would really appreciate if you post your impressions if you have the system running this way. J_Bell |
Follow us on