2/17/2018 8:13 AM | |||||||||||||
Joined: 12/18/2014 Last visit: 10/1/2023 Posts: 30922 Rating:
|
Delivery release for SIMATIC S7-1500 Starter Kit with Technology CPU 1511T-1 PN Anniversary edition "60 Years of SIMATIC": SIMATIC S7-1500 Starter Kit with Technology-CPU 1511T-1 PN Easy entry with the Technology CPU Starter KitThe well-known SIMATIC S7-1500 starter kit portfolio is extended by a new version with technology CPU. Siemens is celebrating 60 years of SIMATIC in 2018. On this anniversary this starter kit will be extended with TIA portal Options. Aniversary bonus: In addition to STEP 7 Professional V15, licenses for the option packages SIMATIC ProDiag S7-1500 for 250 supervisions and SIMATIC OPC UA S7-1500 Small for secure, reliable communication independent of vendor and platform are currently included. SIMATIC S7-1500 Starter Kit with compact CPU:
Note: 1)Full version of STEP 7 valid for 365 days. During this time, all features of the full version are available, and updates and service packs can be installed. At the end of this trial period, the software can be upgraded to a regular version by purchasing a Powerpack in combination with a software update contract (SUS).
|
||||||||||||
Last edited by: Jen_Moderator at: 2/19/2018 12:42:37 PMOptimized link. |
|||||||||||||
This contribution was helpful to
3 thankful Users |
Follow us on