12/27/2018 5:09 PM | |
Posts: 2 Rating:
|
What is the PN Option board you are referring to? Looking for a GSD file for the Deprag AST11 Controller. Need to transmit Real and Dint values. |
12/27/2018 5:49 PM | |
Joined: 7/7/2010 Last visit: 3/10/2025 Posts: 15721 Rating:
|
From a google search, the catalog came up here: https://www.deprag.com/fileadmin/bilder_content/emedia/broschueren_pics/emedia_schraubtechnik/D3165/D3165en.pdf It refers to a specific model / part # for PN, AST6-1 PN / 428001C. If you do not have that specific model, you can add PN to your AST6-11 using an option board. See page 6 where it shows PN option board part # 428010B GSDML files for PN and GSD files for profibus (PB) are to be obtained from the manufacturer of the device. You will not find them on this site.
|
science guy |
|
This contribution was helpful to
1 thankful Users |
3/20/2019 2:22 PM | |
Posts: 5 Rating:
|
I am also looking for GSD file for AST11. Do you have GSD, please ? Thank you |
3/20/2019 2:35 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi F!go, haven´t you just read the last entry from huggy_d1? AST11 has no GSD-file, because it is not with an DP- or PN-interface by default. There must be any additional interface-module or something like that? I can not find anything on the manufacturer-homepage. The AST11 has this features:
There is no interface for Profibus or Profinet for what you would need a GSD(ML) file. I was also looking in the data-sheet posted by huggy_d1. there´s an article-no. of additional interfaces for Profibus and Profinet. But I can´t find anything on the manufacturer-homepage. If I were you, I would start a Support-request on Deprag-Page. hope this helps, regards, |
Last edited by: mopS04 at: 3/20/2019 2:44:22 PMFCK WAR! |
|
This contribution was helpful to
1 thankful Users |
4/18/2022 4:07 PM | |
Joined: 1/28/2022 Last visit: 4/18/2022 Posts: 1 Rating:
|
Hello, could someone solve this? |
Follow us on