3/7/2015 11:11 AM | |
Posts: 1058 Rating:
|
Have a look here: SIMATIC Bus links DP/PA coupler, active field distributors, DP/PA Link and Y Link see Diagnostics with STEP 7: DP/PA coupler FDC 157-0 regards |
3/8/2015 5:57 PM | |
Posts: 9 Rating:
|
Thanks for your reply! I have gone through your suggested link & found valuable information. but i have some queries 1) how can i read diagnostic? 2) how i can disable or enable the following diagnostics:
For more information click on below link https://support.industry.siemens.com/cs/mdm/1142696?c=29935500811&lc=en-WW 3) Is it possible to read Local Life List? As I am using DP/PA link not DP/PA coupler. for more information click on below link https://support.industry.siemens.com/cs/mdm/1142696?c=29935636875&lc=en-WW Thanks. |
3/12/2015 8:14 PM | |
Posts: 9 Rating:
|
Hi, Finally It is done. As i used IM153-2 DP/PA link , I did logic with SFS 13 for reading diagnostic of IM 153-2. Also we can use SFS 51 With SZL_ID = B4. Here is link with example https://support.industry.siemens.com/cs/mdm/1142696?c=29935337739&lc=en-WW From read diagnostic data, Bytes from 120 to 135 I can detect which slave is performing communication with IM 153-2. Thanks For You Help eisenpferdreiter !! |
Last edited by: simply best at: 3/14/2015 2:31:20 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on