11/14/2017 3:44 PM | |
Joined: 9/14/2017 Last visit: 3/26/2025 Posts: 13 Rating:
|
Hi, I am develop a SCADA project in TIA Portal v14 professional. I have face some problem in wincc(PC System) that 1. I select a clock from Toolbox>Elements>clock and drag to screen, then clock is running and show computer set time but when play runtime to "Download to device or start simulation. but it did not show in runtime. 2. I configure "User Administration" and want to displaying user name in scada page. i use a block toolbox>Control>user view and drag to screen and play runtime its not shown in runtime, also invisible some graphic object. N.B. : I am use user administration in panel view KTP1200 It,s work well. 3. I have to clarification a point. If i connect Server PC System(Development Software & SCADA runtime) with CM module, what it will works? Need Solution of this problem. Thank You, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2017 3:04:22 PMNew subject after splitting |
|
11/20/2017 9:23 PM | |
Joined: 4/28/2015 Last visit: 2/20/2025 Posts: 1 Rating:
|
I have the same problem. Any solution? |
3/14/2018 8:47 AM | |
Joined: 8/3/2009 Last visit: 4/24/2025 Posts: 15350 Rating:
|
Hello together I Think this FAQ will help you: https://support.industry.siemens.com/cs/de/en/view/109749283 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on