2/8/2011 3:21 PM | |
Joined: 4/24/2006 Last visit: 3/17/2025 Posts: 8896 Rating:
|
Hello, Do you mean using Profibus DP? Perhaps this link might help: http://mcliterature.danfoss.com/WebPublish/doc_MN33A102.pdf Best regards, Wizard |
2/15/2011 12:48 PM | |
Posts: 4 Rating:
|
Bonjour Je veux établir la communication entre le variateur FC300 et l’automate S7-300 par profibus, j’ai téléchargé l’exemple dans le site de DANFOSS (ftp://software.danfoss.com/drives/Software/Fieldbus/Profibus/pcablockdescription.zip) La communication entre le variateur et l’automate se fait par un câble Profibus violet avec deux fils rouge et vert VERT (PIN 3) -------63 ROUGE (PIN 8) --------62 Et je n’arrive toujours pas à les faire communiquer, ma question c’est comment faire le paramétrage du variateur.J’attend votre réponse merci ??? ----------------------------------------------------------------------------------------------------------------- Hi I want to establish communication between the drive FC300 and S7-300 via profibus; I downloaded the example in the site of DANFOSS, (ftp://software.danfoss.com/drives/Software/Fieldbus/Profibus/pcablockdescription.zip) Communication between the controller and FC300 is via a purple Profibus cable with two red and green wires. GREEN (PIN 3) -------63 RED (PIN 8) --------62 And I still can not connect them; my question is how I can parameter my FC300, please I am waiting for your help ???? |
2/16/2011 8:20 AM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
Hello, And in Danfoss's site have explanation how to do this. Look at MG33C402 and MG33MA22 Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
2/19/2011 10:26 AM | |
Posts: 4 Rating:
|
Good morning My project goal is to read and write via the drive FC300 from S7-300, For this I downloaded the project developed by DANFOSS here is the link: (ftp://software.danfoss.com/drives/Software/Fieldbus/Profibus/pcablockdescription.zip) my problem , I can't read and write the Parameter from the variateur,I tried to simulate the program I downloaded from the site DANFOSS, I described the steps simulation program attachments,Attachments: Problem EXCHANGE AttachmentProblem EXCHANGE.zip (380 Downloads) |
Last edited by: rajraji at: 2/19/2011 10:28 AM |
|
2/19/2011 10:37 AM | |
Posts: 4 Rating:
|
Good morning for more explanation, I sent the Projet attenchement :Programme SIEMENS AttachmentProgramme SIEMENS.zip (633 Downloads) |
Follow us on