3/24/2011 1:48 PM | |
Posts: 3 Rating: (0) |
Please who can help me... I need to know the diference between CPU 946 and 947. |
3/24/2011 4:52 PM | |
Posts: 376 Rating: (57) |
Hello, some information ( manual and product information) about the CPU 946/947finds you here. Manual S5-155U Programmable Controller (CPU 946/947). http://support.automation.siemens.com/WW/view/en/19064665 and here: http://support.automation.siemens.com/WW/view/en/4133837 I hope this information helps you. Best Regards Gucci |
3/24/2011 5:40 PM | |
Posts: 3 Rating: (0) |
Thanks a lot. And you know if I have the same performance using CPU S7-319-3 to replace the two CPU's S5-496/497? |
3/24/2011 11:43 PM | |
Joined: 9/27/2006 Last visit: 10/15/2024 Posts: 12287 Rating: (2685) |
Hello Oswald; I have no doubt that you could get better performance from the CPU 319-3PN/DP that the S5-155U CPUs you asked about. Although the S5-155U was considered very high-end processors of their generation, technology has evolved much in nthe past 20 years and newer generation CPUs are faster, more powerful, and have much larger memory potential. Compare the performance details for the CPU 946/947 (extracted from the manual suggested earlier): CPU 946/947 Product Summary Performance features In the S5-155U programmable controller the CPU 9461947 can be used in single and in multiprocessor mode. It is designed for fast processing of all STEP 5 operations. With a maximum of 896 kbytes this CPU offers a large memory capacity. The most outstanding features are: · Max. 896 kbyte memory for data and user programs, as RAM and for EPROM. ·128 kbyte RAMS are already integrated in the CPU. · 2048 flags · 32768 S flags - 256 timers - 256 counters Processing from up to 4096 binary inputs/ outputs each, 192 analog inputs/ outputs each. Via special interface modules up to 520 000 digital inputs/outputs each or 32 000 analog inputs/outputs each is possible. Programming language and program processingUse the STEP 5 programming language to program the CPU 9461947. The types of representation for STEP 5 are the ladder diagram (LAD), control system flow chart (CSF) and statement list (STL). Furthermore GRAPH 5 is available which is used to program sequential controls (step sequences). The CPU 9461947 allows user programs which are cyclic, alarrn-controlled, time-controlled (max. 9 clock grids). A hardware clock is also integrated. The average processing time of 1 K instructions is |
Last edited by: dchartier at: 3/24/2011 11:59 PM |
|
Follow us on