1/3/2015 1:31 PM | |
Joined: 11/21/2007 Last visit: 3/31/2025 Posts: 2326 Rating:
|
Thanks ChristophD A new boot loader can be written to the CF card using SCOUT via "Options > Write boot sector".
--- The D410_2 seems to have accepted the CF card with changed boot sector. We will now try to download the program and see what happens.
AttachmentCompatibility_SIMOTION_V43123_V4402.pdf (526 Downloads) |
There is no such thing as the last bug in a program |
|
1/4/2015 11:13 AM | |
Joined: 5/12/2006 Last visit: 4/17/2025 Posts: 22597 Rating:
|
Hi, yes this is correct. Regards Christoph |
This contribution was helpful to
1 thankful Users |
2/7/2018 7:22 AM | |
Joined: 5/12/2006 Last visit: 4/17/2025 Posts: 22597 Rating:
|
you must rewrite the bootloader |
Follow us on