5/14/2012 11:10 AM | |
Posts: 90 Rating:
|
Hi Does anyone know what the difference between Dry and Wet contactsfora DigitalOutputis? Do they have the same meaning with Switch and Delay? |
5/14/2012 11:24 AM | |
Joined: 5/28/2008 Last visit: 3/24/2025 Posts: 4520 Rating:
|
Hello, Dry contact is voltage free contact. You can get it from a relay output module or via an external relay. Wet contact: I have never hear this. But if you mean non-dry contact, then you should know the control voltage of it. Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to
2 thankful Users |
5/14/2012 11:31 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
hi, dry means normal contact (shorting link)For Di and wet contact means providing or passing some volt/current to DI regards, viral |
5/14/2012 11:40 AM | |
Joined: 7/18/2011 Last visit: 12/6/2024 Posts: 521 Rating:
|
Hi Ariya Man, In addition to previous posts, Wikipedia states the following about wet contact: Wet contacts aremercury wetted, which gives certain operational advantages. Dry contacts means a relay that does not use mercury wetted contacts. Kind regards, BV |
5/14/2012 2:00 PM | |
Posts: 90 Rating:
|
Ok, so what is the difference between an DO module with relay output and switching output? |
5/14/2012 2:08 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, what do you mean by switching output? All digital outputs are switching. Relais outputs have contacts like a switch, you have to provide a supply to one of the contacts, othe one provides then your supply when activated. Transistor outputs provide + 24V when activated . I suggest you have a look at [url=http://support.automation.siemens.com/CN/view/en/8859629] S7-300 Module Data[/url] to read more about dif output modules. Regards, Marcjan |
Last edited by: Marcjan at: 5/14/2012 2:08 PMProblem solved? |
|
5/14/2012 2:28 PM | |
Posts: 90 Rating:
|
this is what i read in a book recetly. it has divided DO modules with two different outputs, relay and switched.... and im wondering why? |
Last edited by: Ariya Man at: 5/14/2012 2:29 PM |
|
5/14/2012 3:03 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Well i suppose that by switching outputs the mean the Transistor outputs. These outputs provide a voltage at the outputs. Regards, Marcjan |
Problem solved? |
|
5/21/2012 12:23 PM | |
Posts: 103 Rating:
|
in very simple terms: If the field device itself is capable of providing the contact voltage reqired to detect an input then the contact on the module end is called the dry contact. Alternately, if we provide the contact supply to the field and the device in the field is a passive device then it is called the Wet Contact. |
This contribution was helpful to
1 thankful Users |
5/21/2012 7:01 PM | |
Posts: 947 Rating:
|
in additional: DO module with relay output make full break or full contact. But DO module with switching output retain the remainder of resistance. With relay output modules have a limited number of switches. |
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on