6/14/2015 5:04 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Please have a look our Expert Marcjan: https://support.industry.siemens.com/tf/WW/en/Posts/105877 MC (Big blue card) |
Last edited by: Ste39 at: 6/14/2015 5:07:15 PM |
|
This contribution was helpful to1 thankful Users |
6/23/2015 10:58 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello all, SIMATIC memory cards released for S7-400 are not suitable for S7-300. and vise versa. Please note that S7400 Memory cards have different dimensions than that for S7-300. For S7-300, Dimensions: WxHxD in (mm) = 7 x 57 x 45 mm For S7-400, Dimensions: WxHxD in (mm) = 7,5 x 57 x 87 mm. Please find here the following FAQs and you will found the suitable MC for each CPUs in part numbers: Which memory cards can you use with a S7-400 CPU? |
Last edited by: Ayman Elotaify at: 6/23/2015 11:08:36 AMAyman Elotaify |
|
7/5/2015 1:45 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Ayman, Apart from the size that we know are not equal, it is whether the MC for S7-400 works for S7-300 Tomorrow I order a MC for S7-400 and i will try it with S7 -300 if it works , I'm curious |
Last edited by: Ste39 at: 7/5/2015 4:52:47 PM |
|
7/6/2015 9:40 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello, I am not sure if both have same interface or not. In any case, although Siemens stop buying old S7-300 memory cards, you can purshase memory cards compatible with S7-300 old CPUs from "Process-Informatik" http://www.process-informatik.de/produkte/speichermodule&mt=1 |
Ayman Elotaify |
|
Follow us on