Industry Online Support
Technical Forum
4/11/2013 1:40 PM | |
Joined: 4/22/2010 Last visit: 1/15/2025 Posts: 5697 Rating:
|
Hello, Ifyou compare the 2 datasheets: TIME RELAY, CLOCK-PULSE RELAY and
TIME RELAY, MULTI-FUNCTION You will see that the 1555 has only 1 function and the 1505, can be setup for more functions(but not the one the 1555 has). So the question is what function do you need? regards, Marcjan |
Last edited by: Marcjan at: 4/11/2013 1:43 PMProblem solved? |
|
4/11/2013 2:53 PM | |
Posts: 467 Rating:
|
hello, here some more informations: 3RP1555-1AQ30TIME RELAY, CLOCK-PULSE RELAY15 TIME SETTING RANGESAC 24 V DC 100... 127 V,WITH LED3RP1505-1AW30TIME RELAY, MULTI-FUNCTION1 CHANGEOVER, 8 FUNCTIONS,15 TIME SETTING RANGESAC/DC 24... 240 V, WITH LED,SCREW CONNECTION see also the attachment reards LesPaul AttachmentD:\Technical specifications 3RP.pdf (188 Downloads) |
Follow us on