7/25/2013 5:28 AM |
|
Posts: 22 Rating: (2) |
It is 322 |
7/25/2013 5:40 AM | |
Posts: 691 Rating: (36) |
Dear Nandlal Pal Just Bypass the logics to ensure that there is no logic overwritten. |
7/25/2013 5:46 AM | |
Posts: 1064 Rating: (72) |
is all the outputs on one card or just some of them .Make sure that you are not using the qw of the output somewere in your program |
7/25/2013 6:41 AM | |
Posts: 22 Rating: (2) |
When the new card is replaced it is working fine. so that means it is no where overwritten. |
Follow us on