7/9/2013 2:52 PM | |
Posts: 93 Rating: (13) |
Dear Mohmmed Saleh, You have to use intermediate circuit to convert 100VDC to 12/24/05 VD prefarably 24VDC ,because HSC uses 24 VDC .also this intermediate circuitery should have fast switching speed to convert pulses from 5.1 KHz signal. Optocoupler would be easier option for such use. Search this kind of circuit in google. Regards, RKM |
Follow us on