Industry Online Support
Technical Forum
8/1/2008 1:56 PM | |
Posts: 102 Rating:
|
I would recommend to do it either with a C or a Visual Basic script. You can activate them when any of both tags are changed. There is already something in the forum about this topic you can also take a look at it. /tf/WW/en/Posts/5173 |
8/1/2008 2:47 PM | |
Posts: 1275 Rating:
|
Hi, To make properties dynamic you can simply add something to that particular property... If your object is a WinCC object, for instance, a rectangle, access the color properties... To make them dynamic you can use a dynamic dialog, or even a C or VB script. If you have to switch between bitmaps try the Status Display object. You can find further info on all this on the "Getting Started" manual. Best regards, Danielle |
8/1/2008 3:55 PM | |
Posts: 10 Rating:
|
Hi. |
Follow us on