5/10/2012 10:14 PM | |
Posts: 8 Rating: (0) |
Hello! I have a problem with establishing direct connection between WinCC RT Advanced and S7-1200. My OS is Windows 7 Professional. I'm using TIA Portal v11 and I have installed Simatic NET v8.1+SP1. The main problem is that when I want to "Configure PC station online" to establish a connection I can't access the PC station of the target computer. It says that it is locked. Also, when I want to add a module in the Station Configurator it says that it can't be done due to a local S7 connection configuration with COML S7. In attachment You can find some screenshots that discribe the problem. In the HW configuration the PC station and the PC on which I want to run the runtime are the same machine and therefore I assigned the same IP address for both. The name of the PC station and the PC are identical. Both "allow" check boxes are selected in the "Security" menu of the "Configuration Console". Commissioning the drive over the Watch tabel and without the WinCC RT Advanced is working just fine. Could anyone help me to solve this problem? Regards, Nikola AttachmentConfigurations.zip (465 Downloads) |
5/14/2012 11:43 AM | |
Posts: 8 Rating: (0) |
No, I can't generate the XDB file. Do You know what would be the cause of this problem? |
5/14/2012 11:53 AM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Sorry, but no. I've never work with TIA + Simatic.NET. Only used Simatic.NET with Step-7 v5. Never had such problems. I advice to wait a little bit here for other users to respond. If not, you can always try to open Support Request |
Best regards, |
|
5/14/2012 12:31 PM | |
Posts: 8 Rating: (0) |
TIA Portal opened or closed, eitherway the same message appears (screenshot). Even if I turn of all the firewalls allways the same. |
5/14/2012 12:49 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Also try to disable UAC... |
Best regards, |
|
5/14/2012 9:40 PM | |
Posts: 8 Rating: (0) |
O.k. Thank You for your help! Regards, Nikola |
6/8/2017 8:32 AM | |
Joined: 4/18/2017 Last visit: 8/28/2024 Posts: 7 Rating: (0) |
Hello nstojko Did you solve the problem? Best regards, Sergey V. |
Follow us on