11/10/2010 4:31 PM | |||||||||
Joined: 9/27/2006 Last visit: 3/14/2025 Posts: 12344 Rating:
|
Hello dpk; Study the following FAQ; What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server? Siemens proposes the following solutions based on Simatic Net, for an OPC connection over Profibus from a PC: S7 communication (Profibus) S7 communication can only be used for data exchange with S7 stations. You need one of the following SIMATIC NET PC software packages if you want to use S7 communication including SIMATIC NET OPC server for data exchange:
Software:
If you want to do a comparative study on OPC servers for the S7 CPUs, simply search the web, you will find manyofferings from different manufacturers. Hope this helps, Daniel Chartier |
||||||||
Follow us on