6/26/2013 4:36 PM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
Hi, Please find the attachement for the screenshot of CPU 318 2DP Firmware V3.0 specfication where the Activate/Deactivate DP slave is YES. Here is thelinkfor the Technical Specs of the CPU 318 for your information.
|
_______________________________________________________________ |
|
6/27/2013 7:19 AM | |
Joined: 4/17/2012 Last visit: 8/30/2024 Posts: 474 Rating: (10) |
Hi, You got the solution???? It is working???
|
6/27/2013 8:44 AM | |
Posts: 35 Rating: (0) |
hi saravana kumar I found thatCPU 318 2DP Firmware V3.0support theActivate/Deactivate DP slave is YES shown in attachment "untitled". For testing I interface one ET 200m with cpu 318 2dp using profibus and deactivate ET200m using sfc12 using mode 2shown in attachment (OB1) but I got (W#16#F001) RET_VAl of sfc 12 . what is the problem???
AttachmentNew Folder.zip (130 Downloads) |
6/27/2013 9:28 AM | |
Posts: 35 Rating: (0) |
I not use mb15 of mb16 or any bit memory of mw16 range. I also change the memory address of RET_VAl mw50 (even) but i got same problem mw50 value is W#16#F001. |
6/27/2013 9:50 AM | |
Posts: 35 Rating: (0) |
hi Wizard I download Sfc 12 program from the above link.. and change it cpu ---> cpu 318 2dp and change et200m (IM 153-1) as i previously used. when i run this program on my hardware and deactive et200m I observed that RET_VAl => W#16#7002 and W#16#F001 (continuouslyflickering) Busy => high and low (continuously flickering) I attached Hw config file
|
Follow us on