8/26/2022 8:50 AM | |
Joined: 4/8/2021 Last visit: 4/24/2025 Posts: 640 Rating:
|
Hi sadhu67, AFAIK there is no such a option to disable logging process. However, if there is no log defined it's very strange that it check for the logging license. Is the project created from scratch? Maybe if there were logs defined before, even if you have deleted them it still ask from license. In this case I would suggest: 1.Delete IM folder inside folder project following this FAQ as an inconsistent IM folder can have various unwanted effects on your project https://support.industry.siemens.com/cs/ww/en/view/109778709 2. Update ALM to last version available. https://support.industry.siemens.com/cs/ww/en/view/114358 Hope it helps. Br, Cocolino |
Best regards, |
|
8/26/2022 11:51 AM | |
Joined: 9/16/2019 Last visit: 7/19/2024 Posts: 5 Rating:
|
I tried both suggestions but was not succesful. ALM was the latest version. What features use logging ? Alarm View ? |
Follow us on