8/27/2024 11:44 AM | |
Joined: 4/11/2012 Last visit: 9/6/2024 Posts: 181 Rating: (34) |
I created a support ticket to Siemens and got this reply:
So once a F-link connection has been defined, it must be operational or else it will generate an error that shows up in diagnostics buffer and error led. Workaround would be to use alternative communication method (DP_DP) but it is not suitable for us due to large amounts of data being transferred. I guess I need to create dummy connections so that the unused F-links will appear to work from PLC point of view. |
Follow us on