6/3/2019 6:03 AM | |
Posts: 1 Rating:
|
I am using Step 7 V5.5 on Windows 10 with Virtualbox V6.0.6 and IBHLink V1.45 through ethernet to connect to the S7. The problem is that if i disconnect the ethernet cable and i reconnect it i cannot go online anymore with the S7... Pinging the IBHLink i get no answer from the module. I need to shut down VB and start it again... What i can notice is that when i shut down VB i receive an error from the program ccSvcHst...Any possible solution? Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: Pelliccia at: 06/03/2019 06:39:15Last edited by: Jen_Moderator at: 06/03/2019 07:45:45New subject after splitting |
|
Follow us on