5/31/2014 8:08 AM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
There could be many problems, pls. specify what actually u are facing.
|
5/31/2014 11:06 AM | |
Joined: 4/3/2014 Last visit: 9/9/2022 Posts: 54 Rating: (0) |
If there's no alarm/fault mostly there's parameters mistake . |
5/31/2014 11:10 AM |
|
Posts: 39 Rating: (9) |
Dear..... Thank you very much for your quik response. You are right there was a mistake in parameter ... |
5/31/2014 11:15 AM | |
Posts: 784 Rating: (52) |
Can youexplainthis mistake in parameter? |
5/31/2014 12:32 PM |
|
Posts: 39 Rating: (9) |
DearWago Actully i put a wrong logic for parameter P2106 for external fault thats why it was occuring..
|
5/31/2014 1:06 PM | |
Joined: 1/28/2012 Last visit: 7/23/2024 Posts: 519 Rating: (83) |
DearWago Actully i put a wrong logic for parameter P2106 for external fault thats why it was occuring.. For parameter error P2106, it may show you "TRIP" or "ALARM" (if configured as Alarm) with a fault number "F07860".
|
Regards, |
|
This contribution was helpful to3 thankful Users |
Follow us on