3/31/2025 7:56 AM | |
Joined: 2/17/2020 Last visit: 4/22/2025 Posts: 1251 Rating:
|
Hi, The media control used in Unified Panels is derived from VLC. VLC itself can display RTSP streams. However, Siemens has only system tested and supported embedding URLs which are included in the manual, and RTSP is not one of them. SIMATIC HMI HMI devices Unified Comfort Panels > Add-ons > Media Player Basically, I believe that this could work through a script, but it is not system tested, so functionality cannot be guaranteed. |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
Follow us on