Industry Online Support
Technical Forum
6/4/2011 8:57 AM | |
Posts: 74 Rating: (0) |
Hello Thank you all for your responce. [snip] ... Another question, from your experience, the distance between the belt and PLC Cabinet arround 45 meters is it possible to extend the load cell cables to this far or i should use an ET200M (what i dont like unless if i have to)? Best regards splitted from: what SIWAREX should i use? |
Last edited by: CS Moderator at: 6/4/2011 4:26 PMnew subject after splitting Last edited by: Palestine at: 6/4/2011 9:05 AMLast edited by: Palestine at: 6/4/2011 9:03 AM |
|
6/6/2011 2:55 PM | |
Joined: 1/4/2007 Last visit: 12/5/2024 Posts: 1153 Rating: (175)
|
Hello Palestine, into the manual of the Siwarex FTC module: http://support.automation.siemens.com/WW/view/en/20072206 you can find into the chapter 14.3 the max. distance to the load cells: It is 1000 m. Best regards Siwarexi |
This contribution was helpful to2 thankful Users |
Follow us on