7/27/2018 6:38 AM | |
Joined: 4/23/2010 Last visit: 12/9/2023 Posts: 8071 Rating:
|
Hello, It is possible. Signal modules diagnostic data is stored in data records 0 & 1. By configuration with corsponding OB, SFC. the same can be accessed. Please refer the attached sheet for detailed information of signal modules diagnosis for different events. HTH AttachmentSignal modules diagnostic data.pdf (191 Downloads) |
7/30/2018 7:16 AM | |
Posts: 3 Rating:
|
Thanks guys. I ended up using RALRM to gather diagnostic interrupts and distinguish between the types of faults, however if I have more than 2 faults generated (1 on channel 1 and 1 on channel 2), it only shows the latest fault generated. Is there a way to show both/unlimited amount of faults using RALRM? I used the following link: https://cache.industry.siemens.com/d...g82_v20_en.pdf Cheers, Scott Attachment109480387_Diag82_v20_en.pdf (75 Downloads) |
Last edited by: Jen_Moderator at: 7/30/2018 8:40:35 AMAdded file as an attachment. |
|
7/30/2018 10:40 AM | |
Posts: 1283 Rating:
|
Maybe the above thread will give you some insights about multi error diagnostics. I raised the thread, but unfortunately couldn't find a solution in Central Periphery. In Decentral Periphery, It is possible with some modules for individual channel diagnostics. The above link is just a reference case with S7-1200 with AI module. Maybe it helps to understand something. Just give it a try with reading. Thanks, Jay
|
Follow us on