7/15/2019 3:38 AM | |
Joined: 8/6/2018 Last visit: 1/6/2025 Posts: 23 Rating:
|
Hi Everyone, I have few site with S7-1200 connected to WInCC V7.0 via DNP3 connection. I'm trying to troubleshooting DNP3 connection down. When I wiresharking connection, I can see there is some comm between master and slave but on info tab it showing "Delay Measurement". What does it mean? BTW, I can ping all sites from WInCC and they are connected by L2TP VPN. Thanks. Update: I'm using DNP3 Outstation Simulator from FreyrSCADA instead S71200. DNP3 connection worked properly. So, now Im sure that is is S71200 configuration error not network error. Im attaching DNP3 protocol trace from TIA. AttachmentProtocollTrace.txt (56 Downloads) |
Last edited by: amhaziq at: 07/18/2019 03:21:54 |
|
7/19/2019 12:12 PM | |
Joined: 8/6/2018 Last visit: 1/6/2025 Posts: 23 Rating:
|
Yes. That one. |
Follow us on