6/25/2013 10:17 AM | |
Joined: 10/24/2011 Last visit: 3/9/2023 Posts: 257 Rating:
|
Hello Rated X, Thanks for the Reply. I worked out the program with the local make GSM module and it working fine. Now I will work on MD720 module. I have worked already on MD720 with S7200 (CPU 224XP CN). But I am facing one problem in my logic. When at a time two or more alarms are coming, my logic skips the messages and sends only one SMS. It skips alarms which are coming exactly at the same time. I have attached my program file. Follwing are subroutines for generating alarms in my program; SBR 0 ---- SMS_blocks (SMS blocks are called in this subroutine) SBR 10 ----PROCESS_HMI_ALARMS (Alarms bit generation) SBR 14 ----ON_OFF_BIT Please suggest me what can be done for this. Thanks, Shailesh
AttachmentGSM_program.zip (53 Downloads) |
Last edited by: s_vb at: 6/25/2013 10:19 AM |
|
Follow us on