Industry Online Support
Technical Forum
5/25/2011 8:28 AM | |
Posts: 4 Rating: (0) |
From the session I recently attended For Sinamics Drive, there are some points which I would like to clarify and put forth to the moderators.It is learnt from the Features of Sinamics that We Provide an MMC Slot for the transfer of Code into the Sinamics Drive.Queries
other questions are splitted to Do we have an Data Validation Feature when we copy the data from MMC to the Sinamics?. access and move data only if the data is Valid. We provide an USB Port for Sinamics drive. Do we have any secure protocol for accessing?. |
Last edited by: O_Moderator at: 5/26/2011 11:15 AMnew subject after splitting |
|
Follow us on