1/31/2008 12:25 PM | |
Joined: 8/25/2005 Last visit: 10/5/2024 Posts: 1162 Rating:
|
Hello Brebiou, this FCs are necessary for the communication via PROFIBUS DP using the CP 342-5. Within the following manual S7-CPs for PROFIBUS Configuring and Commissioning you should find information about the FCs. Within STEP 7 using the online documentation you will get information too. Best regards Sabine |
1/31/2008 2:00 PM | |
Posts: 7 Rating:
|
Hello Sabine, It's what I needed, thank you very much But I use a CP 343-1 Lean, that can pose problem to use these blocks with these CP? Best regards Brebiou. |
1/31/2008 2:37 PM | |
Posts: 7 Rating:
|
Okay, I have a CPU 313C 2DP, in slave mode, and i want communicate with a gateway converter Modbus TCP/Profibus (more informations here). But, CPU need to use communication blocks to exchange data with the gateway I think. The goal of the project is to make communicate Modicon Quantum <> CPU313C 2DP via the gateway Modicon Quantum communicate with gateway, thus it remains me has to make communicate CPU313C 2DP with gateway. Best regards Brebiou |
1/31/2008 3:23 PM | |
Joined: 9/27/2006 Last visit: 1/13/2025 Posts: 12325 Rating:
|
Hello Brebiou; Siemens offers a Modbus/TCP solution for the CP343-1, but it is not free. I have attached the user manual so yiou can study it; the part number of the FB Open Modbus/TCP package can be found in the first pages. Hope this helps, Daniel Chartier AttachmentOpen_Modbus_TCP_HB_English.pdf (635 Downloads) |
1/31/2008 8:08 PM | |
Joined: 8/25/2005 Last visit: 10/5/2024 Posts: 1162 Rating:
|
Hello Brebiou, the FCs DP_SEND and DP_RECV is only working with the CP342-5 on PROIBUS DP not with CP 343-1! If you want to communicate via an Ethernet you have to establish an ethernet connection within Netpro and transfer Data using AG_SEND and AG_RECV. Maybe this documentation will help you? S7-CPs for Industrial Ethernet Configuring and Commissioning Good Luck Sabine |
Follow us on