11/1/2011 5:33 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Check it there DP/DP Coupler User Description Version V1.1b 11/1998 There have both files GSD and Type file. Copy the corresponding content in text file and save it as SI8070AX.200 in case of TYPE FILE or SIEM8070.GSD in case of Device Description Data File. Best regards, Hristo Mihalev |
11/21/2017 3:35 PM | |
Joined: 1/31/2011 Last visit: 4/2/2024 Posts: 4 Rating: (0) |
Hello mr. UMENCHO, I'd copied the contents of the appendix "12.2 Appendix B - Type File" , pasted into a text file and saved it as "SI8070AX.200". I'd copied this file into COM ET200 directory together with other .200 files. Opening STEP5 V6.6 and then COM ET200, when configuring a new station, not appear the new component (DP Gateway). What I do wrong? |
11/21/2017 5:39 PM | |
Joined: 1/31/2011 Last visit: 4/2/2024 Posts: 4 Rating: (0) |
I tryed something. The last character before the ".200" must be the language identification letter (D, E, F, I, S). The character before the language identification must be "T" letter. The other 6 characters can be anything. By copying / pasting the text found in "12.2 Appendix B - Type File" and naming the file as "SI8070TE.200" (in this case needs to work in English), "DP-Gateway" appears in the choice menu, but trying to select it, the error "File Too Large" will appear. I'm using COM ET200 v4.0 and STEP5 V6.6. Is this error due to the software version?
|