9/3/2016 7:22 AM | ||
Posts: 2 Rating: (0) |
I have a CPU 417-4 and ET200S IOs and modules have to be hot swappable Does IM 151-8 standard 6ES 71511AA050AB0 support hot swapping feature? Do we have to use High Feature Digital and Analog Modules for hot swapping or are the standard modules support this feature as well please help Regards ------------------------------------------------------------------------------------------ |
|
Last edited by: Min_Moderator at: 9/5/2016 9:50:35 AMNew subject after splitting |
||
9/4/2016 11:35 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello PriyankaSud, As far as I know, the hot swapping features depends on two things: 1- CPU (You have S7-400. Just make sure to load OB83 and all error OBs). 2- ET200 series (ET200S supports hot swapping). Just remember, only one missing module is permitted. If more than one to be taken out at a single time, the station will fail (IM151-1 Standard). Best regards, H-H |