5/3/2019 2:46 PM | |
Posts: 10 Rating:
|
Hello everyone, I want to Connect a PC to an S7-1200 using OPC-UA, I am using TIA-Portal v15.1 ,and simatic net v15 I try to perform my task using this description application https://support.industry.siemens.com/cs/ww/en/view/39960679 first, I want to know if I am using the correct description application? does simatic net v15 that i´am using support OPC UA or just OPC DA ? Best Regards |
Last edited by: Jen_Moderator at: 05/06/2019 10:37:12Optimized link. |
|
5/3/2019 3:10 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello oumaimatia; From Step 7 v15, the S7-1500 CPUs support OPC UA directly as server, from integrated instructions. Delivery release TIA Portal V15.1 https://support.industry.siemens.com/cs/us/en/view/109758794 SIMATIC OPC UA S7-1500 The OPC UA S7-1500 option enables easy connection of any third-party device to the S7-1500 via the OPC UA server integrated in the S7-1500 CPU. The following new functions are available with SIMATIC OPC UA with TIA Portal V15 and firmware V2.5: In addition to the OPC UA server, an OPC UA client is integrated in the CPU and offers the following functions via corresponding OPC UA communication instructions: Method calls as well as reading and writing of data . The free SiOME tool is an editor for defining your own OPC UA information models or mapping existing companion specifications on your SIMATIC PLC. OPC UA Client Library:Access to the OPC UA Server of a SIMATIC S7-1500 via Excel VBA. https://support.industry.siemens.com/cs/us/en/view/109748892 If you need to rreate your own OPC UA client to connect to a S7-1500 OPC UA server, this example can provide guidance: Programming an OPC UA .NET Client with C# for the SIMATIC NET OPC UA Server https://support.industry.siemens.com/cs/ww/en/view/42014088 Hope this helps, Daniel Chartier |
5/3/2019 3:24 PM | |
Posts: 10 Rating:
|
Hello, thank you for your reply. I am using s7-1200 , is it the same case ? Best regards |
5/3/2019 3:41 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello oumaimatia;; Sorry, I had misread the type of PLC you were asking about. The pdf documentation that is included in the following FAQ will answer your question: How do you connect a PC station to an S7-1200 with OPC? https://support.industry.siemens.com/cs/ww/en/view/39960679 3- Procedure for S7-1200 V4 and Higher This chapter shows: x The configuration of a SIMATIC S7-1200 and a PC station in the TIA Portal x The configuration of an S7 connection for data exchange between the SIMATIC S7-1200 and the PC station x S7 access to optimized data blocks With firmware V4.0 and higher the S7-1200 CPU supports S7 connections with access to optimized data blocks. The OPC Server V12 and higher supports communication to an S7-1200 only via OPC UA (OPC Unified Architecture). Here you can use optimized data blocks or standard data blocks. Access to optimized data blocks is preset in the TIA Portal. You need an OPC Client which supports OPC UA in order to access optimized data blocks via OPC UA and for using the OPC Server V12 or higher. This entry shows how to configure an S7 connection between the S7-1200 V4 and the PC station in order to be able to use an OPC client which supports OPC UA. Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on