4/16/2025 7:23 AM | |
Joined: 2/8/2019 Last visit: 4/17/2025 Posts: 7 Rating:
|
Dear expert, Im planning to use WinCC (TIA Portal) V20 Professional SCADA with runtime and configuration capability just like the WinCC 7.5 RC. My question is: Does this license need another license to run the scada? 6AV2103-0XA02-4AA5 SIMATIC WinCC Professional V20, max. PowerTags, engineering software in the TIA Portal; floating license; software and documentation on DVD; license key on USB flash drive; class A; 9 languages: de,en,zh included, fr,es,it,ru,ja,ko as download; for configuration of SIMATIC Panels, WinCC Runtime Advanced, WinCC RT Professional (max. PowerTags) WinCC Unified PC Runtime. please observe product release: support.industry.siemens.com entry ID: 109963793 - - content: set (3x DVD + 1x USB) i mean do i need this license to run it? 6AV2105-0PA02-4AA0 SIMATIC WinCC RT Professional, 102400 PowerTags V20, runtime software in TIA Portal, single license, software and documentation on DVD, license key on USB flash drive, class A, 9 languages: de,en,zh included, fr,es,it,ru,ja,ko as download; please observe product release: support.industry.siemens.com entry ID: 109963848 - - content: set (2x DVD + 1x USB) for Tia Portal Professional V20. Does it include feature to configure WinCC professional. Thank you, |
4/17/2025 11:17 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello sidqiRafi the best overview you have probalby in the orderdata excel list in the delivery release: https://support.industry.siemens.com/cs/ww/en/view/109963793/de Here you can see all available licenses for WInCC professional and WinCC Professional Runtime and also the options Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on