6/18/2009 2:57 PM | |
Posts: 6 Rating:
|
Dear all, I am a student who is still new workingwith PLC, PROFINET and stuff. Does somenone knowhow to mirroring port in/with X204IRT switch? Because when i want to configure it via web based management i gotmessage as shown in the attachmentfile. Or is there any other ways to do it? Looking forward for you reply. AttachmentDoc1.zip (143 Downloads) |
Last edited by: CS Moderator at: 6/19/2009 10:30 AMnew subject after splittin |
|
6/18/2009 10:04 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi Shinchan, Are you using the switch which is configured in Step 7? If this is the case do you use it in IRT Mode or in RT Mode? A possible way to continu is to disconnect your controller, set the mirroring option and put the control on. I have to admit I'm not entirly sure how the behaviour of this feature is with the latest firmware version. What kind of firmware are you using? If it's lower then 4.1 please use the following link to update: Firmware V4.1 and GSDML File for SCALANCE X-200IRT Available for Downloading Since you write that you are a student I guess you want to research ProfiNet IO. To have a closer look at the telegrams you could think about using this device: http://www.profitap.com/But I guess it depends on how far you want/need to go with your project. |
Best regards, |
|
6/19/2009 11:27 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi, With IRT it's not possible to use Port Mirroring. At least not with the latest firmware. |
Best regards, |
|
6/22/2009 11:13 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi, Thanks for this feedback! |
Best regards, |
|
Follow us on